Skip to main content
Visitor II
July 13, 2023
Question

STM32 interfacing with FingerPrint module through USB

  • July 13, 2023
  • 1 reply
  • 1896 views

Hello, I have a device that uses an STM32 microcontroller and has a USB port. I am attempting to create a secure access system for this device using a fingerprint module. My question is whether I can connect any fingerprint module to the device through the USB port and create a fingerprint lock system. Additionally, I am unsure about the process of connecting a fingerprint sensor to a device running a Real-Time Operating System (RTOS).

This topic has been closed for replies.

1 reply

TDK
July 20, 2023

Theoretically, yes, it is possible to connect a non-standard USB device by using the USB in host mode. However, you likely won't find a pre-build example of this and will have to implement the low level USB details yourself, provided those details are even available. It's not going to be as simple as installing drivers as you would do on a PC.

Note that "fingerprint device" is not a standard USB device like CDC, HID, or MSC.

"If you feel a post has answered your question, please click ""Accept as Solution""."