2010-06-04 04:59 AM
STM32_Init.c
2011-05-17 04:53 AM
You need to get a newer startup.s, that includes the additional interrupt vectors that is appropriate for your device.
...DCD RTCAlarm_IRQHandler ; RTC Alarm through EXTI Line
DCD USBWakeUp_IRQHandler ; USB Wakeup from suspend DCD TIM8_BRK_IRQHandler ; TIM8 Break DCD TIM8_UP_IRQHandler ; TIM8 Update DCD TIM8_TRG_COM_IRQHandler ; TIM8 Trigger and Commutation DCD TIM8_CC_IRQHandler ; TIM8 Capture Compare DCD ADC3_IRQHandler ; ADC3 DCD FSMC_IRQHandler ; FSMC DCD SDIO_IRQHandler ; SDIO DCD TIM5_IRQHandler ; TIM5 DCD SPI3_IRQHandler ; SPI3 DCD UART4_IRQHandler ; UART4 DCD UART5_IRQHandler ; UART5 DCD TIM6_IRQHandler ; TIM6 DCD TIM7_IRQHandler ; TIM7 DCD DMA2_Channel1_IRQHandler ; DMA2 Channel1 DCD DMA2_Channel2_IRQHandler ; DMA2 Channel2 DCD DMA2_Channel3_IRQHandler ; DMA2 Channel3 DCD DMA2_Channel4_5_IRQHandler ; DMA2 Channel4 & Channel5