cancel
Showing results for 
Search instead for 
Did you mean: 

STM32-F103RBT6 Heating up

Kalyan12
Associate

Hi,

Can anyone tell me why the STM32F103RBT6 getting heated, When ever I connected to the CPU through the USB port the ST-Link will not showing and the code also not Flashing and getting heated.

Thanks,

Kalyan

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
ONadr.1
Senior III

The MCU is probably destroyed. Most often, this can happen when a higher voltage is applied to a pin, or by short-circuiting pins that are output. Sometimes ESB discharge when handling the board. If the NUCLEO board was brand new and it happened the first time it was plugged in and without any external connections, I would try to claim it.

View solution in original post

3 REPLIES 3
Issamos
Lead III

Hello @Kalyan12 

Can you exactly localise the source of heating in the board.

Best regards.

II

ONadr.1
Senior III

The MCU is probably destroyed. Most often, this can happen when a higher voltage is applied to a pin, or by short-circuiting pins that are output. Sometimes ESB discharge when handling the board. If the NUCLEO board was brand new and it happened the first time it was plugged in and without any external connections, I would try to claim it.

@Issamos It is heated up exactly on micro controller chip(IC).

Regards,

Kalyan