2025-11-21 1:27 AM - edited 2025-11-21 2:01 AM
I am working on a BLDC motor 6-step (trapezoidal) control using a NUCLEO-G474RE controller board and NUCLEO-IHM07M1 (L6230) power board with a 48V supply.
Below is my phase activation for one commutation step:
The L6230 gate driver IC overheats quickly, even though I am running only an open-loop 6-step sequence.
Switching frequency: 9 kHz (tested from 8 kHz up to 50 kHz)
PWM duty cycle: ramping from 10% → 40%
Step duration: ramping down from 60 ms → 20 ms
Changing commutation step duration (15 ms → 60 ms)
Slower and faster duty-cycle ramp
Changing PWM switching frequency
Verified PWM compare values and GPIO logic for each step
Even at ≤ 20% duty, the L6230 driver gets noticeably hot within a short time.
Is there any issue with my 6-step commutation logic for the IHM07M1?
Does the L6230 require a specific PWM strategy (e.g., high-side PWM vs low-side PWM)?
Could mis-timed enable/disable of the high-side and low-side MOSFETs cause shoot-through, resulting in heating?
Has anyone successfully implemented 6-step open-loop control on this board with a similar setup?
What are the possible reasons for the L6230 driver to overheat even at low duty cycles and moderate load?
Any suggestions or insights will be greatly appreciated. I want to ensure the commutation sequence and PWM method are correct to avoid stressing the L6230 driver.
2025-12-17 6:38 AM
Hello @Esakkimuthu,
You can test the 6Step solution provided by the MCSDK tool, available at this link.
Refer to the Pins usage and hardware changes section for information about hardware changes required to resolve signal hardware conflicts.
2026-01-12 6:26 AM
Hai Esakkimuthu,
Jayaraj Anbalagan here, from Bangalore.
Kindly share ur mail ID. Me too got stuck in the same point of L6398 inversion in IHM08M1.
Want to know some technical clarifications.
jayaraj.a@gdembsolutions.com
2026-01-13 1:14 AM
Hai Jayaraj,
Thanks for reaching out.
Yes, I’ve worked on the L6398 inversion issue in the IHM08M1 and understand the confusion around it. We can definitely discuss the technical details and clarifications.
You can reach me at:
esakkimuthuk19@gmail.com
Feel free to drop your questions, and we can take it forward from there.
Regards,
Esakkimuthu
2026-01-13 5:22 AM
Sir,
Thanks for ur reply.
My mail ID: jayaraj.a@gdembsolutions.com/ 92422 85979.
Sent a mail to you. Kindly check and reply me.
Jayaraj.A
2026-02-06 8:29 AM
Sir,
Busy..
Where are you located? KA or TN or AP?