cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Connectivity line USB device Isochronous IN transfer

dserserg
Associate II
Posted on November 29, 2009 at 08:04

STM32 Connectivity line USB device Isochronous IN transfer

2 REPLIES 2
dserserg
Associate II
Posted on May 17, 2011 at 13:32

Hello.

I explained the problem

http://www.st.com/mcu/forums-cat-8613-23.html&start=18

with v3.1.0 RC1 of USB library. But it seems nothing has changed in the final version.

There is isochronous buffer only for OUT transfer in USB library, and I can't get IN transfer to work. Maybe someone had deal with it? I just need a correct example.

[ This message was edited by: dserserg on 29-11-2009 12:35 ]

dserserg2
Associate
Posted on May 17, 2011 at 13:32

Now link is [DEAD LINK /public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/ARM CortexM3 STM32/STM3210C-EVAL USB Driver&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E&currentviews=4319]here.

Problem is still actual.