2017-05-11 12:25 AM
Hi to everyone,
I am a newbie in STM32 programation and I m not actually sure that is the right way to ask my question...
I hope I can find some help because I have some issues just for basic stuff.
Here is a little description : I have a STM32F405 board with a battery integrated and the voltage measure is plug on the PA2 entry of the board. After some search on internet, I am using ADC to read that measure and the return value is 4 In the first place, I thought that was done but when I let the battery discharge itself, the return value still is 4..
Can you explain me what's wrong in my code or eventually show me some documentation ?
int main(void)
{ int ConvertedValue = 0; adc_initialize(); while (1) { ConvertedValue = adc_convert_bat(); printf('Value battery : %d\n', ConvertedValue); } }int
adc_convert_bat() {ADC_RegularChannelConfig(ADC1, ADC_Channel_2, 1, ADC_SampleTime_144Cycles);
ADC_SoftwareStartConv(ADC1);
while
(!ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC));return
ADC_GetConversionValue(ADC1); }void
adc_initialize() {ADC_InitTypeDef ADC_init_structure;
GPIO_InitTypeDef GPIO_initStructre;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1ENR_GPIOAEN, ENABLE);
GPIO_initStructre.GPIO_Pin = GPIO_Pin_2;
GPIO_initStructre.GPIO_Mode = GPIO_Mode_AN;
GPIO_initStructre.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOA, &GPIO_initStructre);
ADC_DeInit();
ADC_init_structure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_init_structure.ADC_Resolution = ADC_Resolution_12b;
ADC_init_structure.ADC_ContinuousConvMode = ENABLE;
ADC_init_structure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1;
ADC_init_structure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_init_structure.ADC_NbrOfConversion = 1;
ADC_init_structure.ADC_ScanConvMode = DISABLE;
ADC_Init(ADC1, &ADC_init_structure);
ADC_Cmd(ADC1, ENABLE);
}Thanks to you all and sorry if the message is send at a wrong place...
Nico-
2017-05-11 2:48 AM
Hello Nicolas,
It seems that your adc_initialize () function is incomplete.
You must also configure the channel (PA2 = ADC1 Channel 2) after ADC_init()
ADC_RegularChannelConfig() configure ADC Sample time.
...
ADC_Init (ADC1, & ADC_init_structure);
ADC_RegularChannelConfig (ADC1, ADC_Channel_2, 1, ADC_SampleTime_3Cycles);�?�?
ADC_Cmd (ADC1, ENABLE);
...�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-05-11 7:11 AM
Thank you it seems to work fine.
I was actually doing it after the ADC_Cmd which seems to be the error.
Well it's working now, thanks you !
2017-05-11 8:29 AM
Hi
Bousmanne.Nicolas
,Thank you it seems to work fine.
https://community.st.com/0D50X00009bMM5DSAW
-Nesrine-