2015-07-05 5:26 AM
Hi friends, looking for any project based on STM32F105 which can copy (Transfer) files from USB stick to On board SD card repeatedly. May be such a device can be used to batch copy files from USB stick to SD card without any Computer.
2015-07-05 6:10 AM
Probably wouldn't do it with the F105, given the choice.
The STM32F4-DISCO has code examples for USB-MSC reader, there's SDIO code, and FATFS implementation. To clone/copy a card you'd need to write some code to enumerate the files/sub-directories and copy/create them one at a time between the media.2015-07-05 1:25 PM
Hi clive1,
why not STM32F105 as it USB FS Core and Native SDIO interface with DMA Support.2015-07-05 4:36 PM
You can build your project with whatever part you want.
I think there are other parts, which are faster, have more memory, and more available/working code.2015-07-06 1:48 AM
Ok, i will try to implement the concept with STM32F105 (Cheapest one with USB FS host & SDIO).