cancel
Showing results for 
Search instead for 
Did you mean: 

STM32C092 and CAN FD transceiver selection

Nimit Vachhani
Associate III

Greetings Everybody,

I am trying my hands with CAN FD. I have selected STM32C092RC for the same application as it has can fd port.

I was wondering if MCP2561/62 can fd transiver ic works with this controller. Please advice. I was also looking for schematic and cad resources for NUCLEO-C092RC board, but cant find. If anybody has the link for cad resources and schematics for NUCLEO-C092RC board then please do forward it.

Thanks in advance.

1 REPLY 1
mƎALLEm
ST Employee

Hello @Nimit Vachhani ,

1- MCP2561 is OK. But please select the version having VIO pin. But becarefull this transceiver could not exceed 1Mb/s if you are planning to use CAN-FD data rate > 1Mb/s:

mALLEm_0-1741092613977.png

If you plan to exceed that bitrate, I may suggest MCP2562FD that can reach up to 8Mb/s.

2- For the schematic and cad resources for NUCLEO-C092RC board, they are not yet available on the ST website.

It will be available soon. For the moment, you can rely on the UM3353

Edit: NUCLEO-C092RC has already a CAN-FD transceiver:

mALLEm_0-1741093798048.png

No need to add another CAN transceiver. 

And this is the CAN connector (in green) correspond to CAN_H and CAN_L + GND (I think):

mALLEm_1-1741093849151.png

Hope that answers your questions.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.