cancel
Showing results for 
Search instead for 
Did you mean: 

STM Virtual COM Port not working in windows 11

Neeraj
Associate II

Dear ST Community,

 

I'm using Windows 11 on my PC but the device manager doesn't detect the STM32 USB VCP. Please help me fix this issue.

best regards

Neeraj

8 REPLIES 8
AScha.3
Chief III

Hi,

what happens , when you connect to PC/USB ? 

If nothing at all, try other USB cable (with data lines), maybe you have a charger cable now ...

If you feel a post has answered your question, please click "Accept as Solution".
Neeraj
Associate II

I changed the cable, but the issue remains the same.

Neeraj
Associate II

Neeraj_0-1713436513389.png

I am using CDC Lib for sending messages.

Please use this button to properly post source code - not as images:

AndrewNeil_0-1713437233933.png

 

Does anything happen at all on the PC when you plug in? eg, does it see any "unknown" device? or report any error?

Presumably, your embedded code should also detect when it's plugged in - is that happening?

 

 

Neeraj
Associate II

Nothing happening at the PC End

So what about the STM32 end?

What debugging have you done to see what's happening there?

i have the exact issue but when i connect the usb it says usb device not recognized on my pc end 

So that's not the exact issue, then - is it?

In @Neeraj's case, nothing at all happens on the PC;

In your case, something does happen - so yours is a different issue.