cancel
Showing results for 
Search instead for 
Did you mean: 

STM Virtual Com Port Driver for Windows 10

gaurav2
Associate II
Posted on June 04, 2016 at 01:21

I downloaded the VCP_V1.4.0_Setup.exe and ran it. But it only has Win7 and Win8 directories. 

Does anyone if either of them will work on 64-bit Windows 10? If neither will work then where can I get the STM VCP driver for Win 10?

Thanks!
4 REPLIES 4
mark239955_stm1
Associate II
Posted on June 04, 2016 at 08:54

I got one of them working (sorry, can't remember which) on Win10 a few days ago.  It didn't auto-detect, I had to muck around and ''have disk'' etc but it did work.

slimen
Senior
Posted on June 23, 2016 at 11:19

Hi,

Please confirm if this problem still persists?

May be compatibility mode can resolve this issue !

Regards

markpdbailey
Associate
Posted on August 22, 2016 at 12:53

The driver files will be installed at 

C:\Program Files (x86)\STMicroelectronics\Software\Virtual comport driver\Win8

Open a command prompt and cd into into this directory

run

dpintst_amd64 /LM

Click yes on the driver installation boxes