cancel
Showing results for 
Search instead for 
Did you mean: 

usart bootloader data section

mats23
Associate II
Posted on August 19, 2016 at 22:11

usart bootloader data section

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
mats23
Associate II
Posted on August 19, 2016 at 22:20

Posted on August 19, 2016 at 22:23

The forum does not support mobile devices well, Android is workable with FireFox.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mats23
Associate II
Posted on August 20, 2016 at 08:20

clive1, I realized that iOS was not at all compatible with the forum. Sorry for posting garbage.

What I was trying to post originally was:

I am programming an STM32F0 device from an STM32F429 DISCO board using the USART system

memory boot mode. I have generated a binary file in TrueStudio, read the file into the device on

the DISCO board and then transferred it byte by byte to the STM32F0 over the USART. When 

writing into the memory of the STM32F0 I start at its address 0x08000000, which I understand

is the start address of the flash. It seems to work well and the STM32F0 seems to be up and

running after the programming, but when looing into the linker file I realize that the .data

section is linked into RAM and not the flash. I understand that .data contains initialized data

and now I cannot understand how I possibly should have managed to get that section into

its right place when programming over the USART.

Do I need to do something special for the .data section when using the USART system 

memory boot, or am I misunderstanding something here?

Thanks!

/M

Posted on August 20, 2016 at 14:18

While the linker allocates/manages resources in RAM, this usually gets tacked on the end of the FLASH image in embedded so that the startup portion of the code can copy this down into RAM, or zero out sections, before it starts running your code. In GNU this is situated in the startup_stm32fxx.s file immediately after the Reset_Handler symbol, in Keil by calling __main, and IAR _cstartup

You should probably look at the .HEX file to see what addresses the linker output is covering. The scatter file or linker script should describe how the load regions are managed, ie RAM content nested inside FLASH.

The boot loader can write data into FLASH or RAM

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mats23
Associate II
Posted on August 22, 2016 at 08:46

I see clive1, thanks for the answer.

/M