cancel
Showing results for 
Search instead for 
Did you mean: 

STM Studio: variables sample rate

elil
Associate III
Posted on September 06, 2011 at 22:10

Dear,

What is the sample rate of variables in STM Studio ? In one of the application notes I found 5msec, but I'm not sure if it is correct. 5msec is too slow. Is that possible to increase/decrease the rate in the STM studio ? I didn't find this option.

Thanks

#stm-studio #discovery #stm32f4 #e
1 REPLY 1
evgen
Associate
Posted on January 29, 2014 at 10:37

I am using STM32F4 Discovery. I would like to know if there is an example showing using SoftTrace together with STM Studio. Currently STM Studio offers example for KEIL and STM32f10x

And what transfer speed/sample rate could be expected using that option of dumptrace? Now sample rate is around 100 samples/s. What kind of transfer rates could be expected with other debugger interface besides SWD?

Best regards, Evgen