cancel
Showing results for 
Search instead for 
Did you mean: 

Still have problems with supplying nucleo L432KC from external source

xpp07
Senior

I updated the ST Link firmware, and followed the sequence described in the User Manual. But the sequence says I have to connect the PC, and I don't want to. I just want the controller to run its program without connecting the USB, using a 5V supply connected to the 5V pin.

4 REPLIES 4

Perhaps keeping this in the old thread would have been better.

Have you removed SB1 ?

Make some very simple code that toggles PB3

Does it work if you use a USB attached battery pack or charger?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
xpp07
Senior

Yes, SB1 is removed. For the nature of my project, it wouldn't work to use a charger o USB attached battery pack. But, if that's the only solution, I will have to see what I can do.

It is suggested as a method of diagnosing the issue. You should be able to blink an LED attached without connecting to a PC. I'd have to invest a bunch of time to prove that I could do it.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
xpp07
Senior

I've connected the 5V pin to 5V pin of the USB connector through a wire. That way it works.