cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-IHM022V1

dominik
Senior
Posted on May 10, 2013 at 09:27

Hi

I'm interesting to use the STEVAL-IHM022V1 Evaluation Board to drive 2 BLDC DC Motors from Maxon with Encoder and HallFeedback (3pole 24VDC 40W). I need to drive them in sine modulation with the FOC control.

Now which power stage board should I use? Is there some evalaution board from ST to use?

The other question I have is the positioning mode. I need to drive the moltor with a speed x to the position y. Is this part implemented in the STM32 Dual FOC MC Software library?

Regards, Dominik
0 REPLIES 0