2015-05-07 8:54 AM
Hello,
I have managed to compile and run the stm32cubef4 libs, together with STemWin V5.26. I use the STM324x9I-Eval board with MB1046B display board. I can run all the included examples, plus the sample available on the Segger site. The one i try to use in my project is ALPHA_Bargraph. It seems to run fine, with the exception of the 'Draw alpha effect': Rect.x0 = xPos; Rect.x1 = xPos + 3; Rect.y0 = yPos; Rect.y1 = yPos + 122; GUI_SetClipRect(&Rect); GUI_SetColor(0xd99100); GUI_SetAlpha(168); GUI_FillRoundedRect(xPos, yPos, xPos + 172, yPos + 122, 4); GUI_SetClipRect(NULL); GUI_FillRect(xPos + 4, yPos + 1, xPos + xBlend, yPos + 122 - 1); GUI_SetAlpha(0); Commenting out the above code seems to speed up the displaying of the bar elements, but when enabled i don't see the blue rectangle that moves in the foreground when i run the Windows executable for this sample. I have tried to check the configuration values, increase the available RAM for the library, etc, with no luck. Here some of those settings: #define GUI_NUMBYTES (1024) * 1024 unsigned long *mem = (unsigned long *)0xC0000000; .... GUI_ALLOC_AssignMemory(mem, GUI_NUMBYTES); .... #define GUI_NUM_LAYERS 2 #define GUI_OS (0) #define GUI_SUPPORT_TOUCH (0) #define GUI_SUPPORT_MOUSE (0) #define GUI_WINSUPPORT (1) #define GUI_SUPPORT_MEMDEV (1) #define GUI_SUPPORT_DEVICES (1) .... define XSIZE_PHYS 480 #define YSIZE_PHYS 272 #define NUM_BUFFERS 2 /* Number of multiple buffers to be used */ #define NUM_VSCREENS 1 /* Number of virtual screens to be used */ #define GUI_NUM_LAYERS 2 #define LCD_LAYER0_FRAME_BUFFER ((int)0xC0200000) #define LCD_LAYER1_FRAME_BUFFER ((int)0xC0400000) Maybe there is an extra configuration somewhere i have missed ? Thank you. Regards, Chris2015-05-09 6:24 AM
Ignore that, seems the LCD driver in the stm32cubef4.zip package is a work in progress(read not working). Alpha blending not implemented.