cancel
Showing results for 
Search instead for 
Did you mean: 

stdio via USB virtual COM port

lanchon
Associate III
Posted on April 04, 2009 at 17:08

stdio via USB virtual COM port

This discussion is locked. Please start a new topic to ask your question.
48 REPLIES 48
pandoraems
Associate II
Posted on May 17, 2011 at 12:28

well, i feel like a fool now

the only change i made and completely forgot that i made it (that evidently caused things not to work) was commenting out that one line (mentioned by someone earlier in the thread).

thanks for having patience with me. It works now!

killgi
Associate II
Posted on May 17, 2011 at 12:28

Hi, I want to control my device via Usb. And I think that library can help me. But my toolchain based on IAR EW-ARM 5.2 (on WindowXP pc) and I have problems with integration into my environtment - errors during linking process:

Code:

Error[Li005]: no definition for ''USB_Init'' [referenced from C:Documents and

SettingsAlfiyaÌîè äîêóìåíòûICtest_icVCPprojSTM3210B-EVALObj

main.o]

Error[Li005]: no definition for ''__cs3_interrupt_vector'' [referenced from C:

Documents and SettingsAlfiyaÌîè äîêóìåíòûICtest_icVCPproj

STM3210B-EVALObjmain.o]

Error[Li005]: no definition for ''NMIException'' [referenced from C:

Documents and SettingsAlfiyaÌîè äîêóìåíòûICtest_icVCPproj

....

And so on

71 Errors

:-[

http://rapidshare.com/files/214108747/VCP.rar.html

my project

mlg7
Associate II
Posted on May 17, 2011 at 12:28

>Error[Li005]: no definition for ''USB_Init''

> [referenced from C:Documents and SettingsAlfiyaÌîè äîêóìåíòûICtest_icVCPprojSTM3210B-EVALObj main.o]

At first, I see Cyrillic letters in the path, at second,

I don't see slashes / or backslashes \.

At 3rd, you may try to type in some arbitrary text into

the file containing the function that cannot be found,

say, ''sdfljk adfljkfg asdfj (*&)_ ;;'', and see if

the error will be reported. If it's not reported,

the file is not compiled.

andreas2
Associate II
Posted on May 17, 2011 at 12:28

There's a ''__cs3_interrupt_vector'' in there, which suggests that you're trying to use something for CodeSourcery's GCC in IAR, likely some startup file or something like that.

pitman
Associate
Posted on May 17, 2011 at 12:28

The forum seems to have lost the attachment for this code.  Would it be possible to re-post it?

saimaddy123
Associate II
Posted on May 17, 2011 at 12:28

Did any one has this working on Olimex STM32-H107?

Timo- the code is still there on first post in the thread. look into attachments above the post..

saimaddy123
Associate II
Posted on May 17, 2011 at 12:28

I could have it working for STM32F107VCT6. Reference design is olimex STM32-H Posted the code here... Let me know if you guys find any problems with it...

https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM CortexM3 STM32/stdio over USB serial in STM32-H107&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E&currentviews=87

alexborysevych9
Associate II
Posted on August 08, 2011 at 12:36

Can anyone re-attach project source code once again, pls! There are no attachments in current topic(

giu
Associate II
Posted on December 06, 2011 at 17:54

Could you repost the file? There is no attachment available anymore

fbl2000
Associate
Posted on December 15, 2011 at 22:16

Hello,

if somebody has a working program file for the olimex STM32-P107, then please upload.