cancel
Showing results for 
Search instead for 
Did you mean: 

stdio via USB virtual COM port

lanchon
Associate III
Posted on April 04, 2009 at 17:08

stdio via USB virtual COM port

This discussion is locked. Please start a new topic to ask your question.
48 REPLIES 48
dion
Associate II
Posted on March 26, 2012 at 14:43

Hello to all,

is it only me who can't find the code in the attachment? it would be great if somebody could upload the code again.

Best regards,

Dion

anderson
Associate
Posted on November 02, 2012 at 12:57

I can't find the attached code. can you provide it?

anderson
Associate
Posted on November 02, 2012 at 12:59

I couldn't find the attached code. could you provided it?

Posted on November 02, 2012 at 13:09

This is a 3 year old thread, before the forum last fatally crashed, the original posters are unlikely to respond.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
viktor
Associate
Posted on January 24, 2013 at 17:49

It also seems to be the only example of an USB virtual serial port for STM32 devices that I could find after extensive googling. It would be nice to get hold of it. Alternately I'd appreciate if someone could point me to a complete USB serial port example I can get to work on the F3 or F4 discovery with minimal effort (I know, I should learn the USB spec but you've got to start somewhere).

asinicki
Associate
Posted on January 25, 2013 at 20:03

There is a link on this forum to a COIDE project that uses the VCP.  It is not perfect but it works and is a good place to start.  I had it working with the STM3241G_Eval board in short order.

http://www.coocox.org/forum/topic.php?id=1757&page=2

esg
Associate
Posted on February 05, 2013 at 08:52

Hello,

i am newbe to STM32.and i am using STM32F103C8T6.i have added the USB Lybrary to my code and it was compilled successfully by the gcc compiler(arm-none-eabi).here when i connected my board to PC with USB i am getting ''Unrecognised device''.is there any thing i need to add code after the ''pProperty->Init();'' function call in the USB_Init() function.I also connected a 1.5K pull up at D+ of USB.please help me out someone.

void USB_Init(void)

{

  pInformation = &Device_Info;

  pInformation->ControlState = 2;

  pProperty = &Device_Property;

  pUser_Standard_Requests = &User_Standard_Requests;

  /* Initialize devices one by one */

  pProperty->Init();

?????????stuck here to add code

}

gguerrero9
Associate
Posted on March 21, 2013 at 14:26

Hi there,

 I am not able to find attached code :-(, would you please post it again?

thanks in advance

Gabriel

Posted on March 21, 2013 at 14:37

I am not able to find attached code :-(, would you please post it again?

 

No kidding?! This thread is pushing 4 years old before the forum last fatally crashed, the original posters are unlikely to respond. I wish we could lock threads to stop getting questions like this.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..