Posted on May 17, 2011 at 12:28>Error[Li005]: no definition for ''USB_Init'' > [referenced from C:Documents and SettingsAlfiyaÌîè äîêóìåÃòûICtest_icVCPprojSTM3210B-EVALObj main.o] At first, I see Cyrillic letters in the path, at second, ...
Posted on May 26, 2009 at 15:03As usual, to enable something you need to switch power on, and to switch the clock on, and turn on the PLL clock, and PLL power, and have HCLK on the right pin, and set the right divisors everywhere... I do not remembe...
Posted on April 13, 2009 at 07:52I have not managed to run the STM virtual com port example when compiled with gcc/winarm, but could do it with evaluation keil. I have inlined Set_system(), Set_USBClock() [this one was empty], USB_Interrupts_Config(...