cancel
Showing results for 
Search instead for 
Did you mean: 

Starting with STM32F0DISCO...''errors''

fbrand
Associate
Posted on September 14, 2015 at 12:25

Hi,

i'm just start working with the Discovery Board STM32F072B.

I've installed CubeMX, the MDK-ARM 5.16a & ST-Link Utility 3.7.0

At first i want to go through the examples of the Disco-Board.

I can start and rebuild targets as described in the ''getting started'' manual.

I also have a running connection via the integrated ST-Link/V2

But...

after rebuild the target files i want to start the debug-session in µvision5 and get get a error-message: ''cannot load flash device description !'' and ''flash download failed - Cortex-M0''

Can someone give me hints, what's going wrong here ?

Are there settings i haven't made etc ?

thanks in advance...
2 REPLIES 2
Nesrine M_O
Lead II
Posted on September 14, 2015 at 14:13

Hi brand.eckhard,

Are there settings i haven't made etc ?

Open your MDK-ARM, go to:  Project > Options for Target >Utilities>Settings>Flash Download>Add Flash programming related to your device.

In your case add: STM32F0xx_128KB Flash 

-Syrine-

fbrand
Associate
Posted on September 14, 2015 at 15:33

Hi Syrine,

thank you ! that solved the problem...