cancel
Showing results for 
Search instead for 
Did you mean: 

Start with STM32F4-Discovery

mosine
Associate II
Posted on June 18, 2013 at 16:22

Hello,

I'm new user. I read many documents, but I have

doubts

. I'm working with uVision. My question is: is it possible load flash memory by mini usb? If yes, How I can configure debug option in uVision?

THANKS

#stm32f4-discovery-usb
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on June 18, 2013 at 18:16

USB connector CN1 provides connection the ST-LINK (SWD Debugger) on the board.

You will need to make sure the ST-LINK driver is installed (\Keil\ARM\STLink)

In Keil, depending on the ST-Link firmware you'd need to pick ''ST-Link (Deprecated Version) or ''ST-Link Debugger'', you also need to ensure you pick ''SWD'' mode in the settings, as ''JTAG'' is not supported.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..