cancel
Showing results for 
Search instead for 
Did you mean: 

Stack pointer is setup to incorrect alignment?

infoinfo987
Associate
Posted on May 10, 2011 at 00:12

Stack pointer is setup to incorrect alignment?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on May 17, 2011 at 14:34

You should probably download and use the VL Discovery board's firmware library, using the classic library for the original STM32F10x parts will probably introduce a bunch of problems with the PLL and Flash Wait States. The STM32F100 only runs at 24 MHz, without wait states, or flash prefetch.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..