2024-08-28 02:01 PM
I have a Arduino Portenta H7 lite and I am using Arduino IDE to program it to read data from VL53L8CX.
I am able to read data over I2C. But for SPI, I am getting the following error
error: no matching function for call to 'arduino::HardwareSPI::HardwareSPI(int, int, int)'
SPIClass DEV_SPI(SPI_MOSI_PIN, SPI_MISO_PIN, SPI_CLK_PIN);
Github code that I am using.
https://github.com/stm32duino/VL53L8CX/tree/main/examples
The HelloWorld_I2C example works well.
The HelloWorld_SPI throws error for SPIClass.
How can I resolve it?