2023-06-29 5:00 PM
I am having trouble connecting ST development boards to my computer. I have tested the following development boards:
B-G431B-ESC1
NUCLEO-G474RE
b-g474e-dpow1
I had trouble connecting when I had Windows 10, I just upgraded to Windows 11 and have the same problem.  All the trouble shooting I have done has been on Windows 11.  
When I plug in to my computer via USB the development board's red light continuously blinks, showing that the board has power.
When I go into device manager, I can not find the COM port for the nucleo, showing that the board is not communicating with the computer.
Steps I have already taken to troubleshoot:
-Tried multiple boards
-Tried 2 different USB cables
-Tried 2 different USB ports (both seem to work with my mouse leading me to beleave it is not the USB port)
-Installed STM32 ST-LINK Utility
      +It could not connect
-Reinstalled the ST-LINK driver  (en.stsw-link009)
      +I ran the install as an administrator and at the end of the install wizard it showed 3 drivers with green check marks next to them, leading me to beleave they were installed
Any further ideas would be greatly appreciated. I