cancel
Showing results for 
Search instead for 
Did you mean: 

ST-LINK Issue - Target unknown error 5010512

Dick Lin
Senior

Hi,

I am seeing the issue since yesterday for unable connect to target. Here is the message from TrueSTUDIO. Unable to connect using STM32 ST-LINK Utility as well.

I am guessing the ST-LINK device burned. We are using tag-connect TC2050 adapter and connector. My question is what might burn ST-LINK? How to know if the ST-LINK device is mal-function?

Thx

http://www.tag-connect.com/Materials/TC2050-ARM2010.pdf

Atollic TrueSTUDIO gdbserver for ST-Link. Version 4.2.2 (WIN32 2018-02-26 16:20:21 15675)

Copyright (c) 2018, STMicroelectronics. All rights reserved.

Starting server with the following options: 

    Persistant Mode      : Disabled 

    LogFile Name        : debug_log.txt

    Logging Level       : 1

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Disabled 

    SWD Debug         : Enabled 

Target unknown error 5010512

Error in initializing ST-Link device.

Reason: Unknown. Please check power and cabling to target.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3

>>How to know if the ST-LINK device is mal-function?

Test it on a working target? Have two so you can compare/contrast?

>>My question is what might burn ST-LINK? 

The buffers, regulators or STM32F1

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Dick Lin
Senior

Found it, the VAPP (target VCC) on the JTAGE 20-pin connector is not right. Issue is on our board. Thx

Khouloud GARSI
ST Employee

Hi @Dick Lin​ ,

Thanks a lot for sharing the solution. For sure, this will be helpful for other users facing the same issue.

Khouloud.