st-link command line utility want not start the application
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-02-09 6:52 AM
Posted on February 09, 2018 at 15:52
Hello! I want to program a STM32L073CB device FLASH and option bytes and then to start the application. If I don't program the option byte I have not problem with the application start. That is the command line:
ST-LINK_CLI.exe -c SWD UR -ME -SE ed1 -V 'after_programming' -P Lora_sx1276mb1mas.hex -HardRst -Q
If I add an option byte value, the hard reset is performed but the application is not started. That is the command line:
ST-LINK_CLI.exe -c SWD UR -ME -SE ed1 -rOB -V 'after_programming' -P Lora_sx1276mb1mas.hex -OB RDP=1 -HardRst -Q
Anybody know how I can program and the option byte and the application then starts successfully?
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0