cancel
Showing results for 
Search instead for 
Did you mean: 

ST Flash Demo - Can it program new parts?

Phillips Jr..Clyde
Associate III
Posted on May 03, 2015 at 19:26

The reason I ask is I made 3 custom ST205 boards. The one board that I  debugged using development tools (JTAG/SWD) and then erased the chip I can program using the ST Flash Demo Utility from my .hex file.

The ST Flash Loader Demo is not recognizing the other boards.

It seemed like I saw this before on the one board I can program, before I used the JTAG/SWD.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on May 04, 2015 at 03:05

With BOOT0 strapped high it should work via USART1 and USART3, as well as USB (via DfuSe)

You could also check with a terminal app, like RealTerm, sending the hex byte 0x7F at 9600 8E1 and looking for an 0x79 response.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..