2017-10-03 10:38 PM
Hello All
currently i am working in Fatfs with stm32f070 with spi1.
when i move to spi2 its not working.
i am trying multiple times but i cant get success.
here is my init function
void SPIFlashInit(void)
{ SPI_InitTypeDef SPI_Struct; GPIO_InitTypeDef GPIO_Struct; uint32_t stat;RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB ,ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA ,ENABLE);GPIO_Struct.GPIO_Pin = GPIO_Pin_15;
GPIO_Struct.GPIO_Mode = GPIO_Mode_OUT; GPIO_Struct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_Struct); GPIO_WriteBit(GPIOA,GPIO_Pin_15,Bit_SET);// Configure SPI1 pins: SCK, MISO and MOSI
GPIO_Struct.GPIO_Pin =GPIO_Pin_13
|GPIO_Pin_14
|GPIO_Pin_15
; GPIO_Struct.GPIO_Mode = GPIO_Mode_AF; GPIO_Init(GPIOB, &GPIO_Struct); //Configure I/O for Flash Chip select // GPIO_PinAFConfig(GPIOB,GPIO_PinSource13,GPIO_AF_0); GPIO_PinAFConfig(GPIOB
,GPIO_PinSource14,GPIO_AF_0); GPIO_PinAFConfig(GPIOB
,GPIO_PinSource15,GPIO_AF_0); //SPI1 configuration SPI_Struct.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_Struct.SPI_Mode = SPI_Mode_Master; SPI_Struct.SPI_DataSize = SPI_DataSize_8b; SPI_Struct.SPI_CPOL = SPI_CPOL_Low; SPI_Struct.SPI_CPHA = SPI_CPHA_1Edge; SPI_Struct.SPI_NSS = SPI_NSS_Soft; SPI_Struct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2; SPI_Struct.SPI_FirstBit = SPI_FirstBit_MSB; SPI_Struct.SPI_CRCPolynomial = 7; SPI_Init(SPI2, &SPI_Struct); SPI_RxFIFOThresholdConfig (SPI2,SPI_RxFIFOThreshold_QF); SPI_Cmd(SPI2, ENABLE);}
please ans me where i am wrong in this code.
Note: this post was migrated and contained many threaded conversations, some content may be missing.2017-10-04 5:37 AM
Hello!
What is your device exactly?
As you can see AF0 SPI2 is available on F070xB devices
Regards.
vf
2017-10-04 8:50 AM
hi,
i am using stm32f070 device. i know that its available on AF0 as you can see in my design. i am using AF0 for SPI2.
in my debug i can see that it will stuck on
FlagStatus SPI_I2S_GetFlagStatus(SPI_TypeDef* SPIx, uint16_t SPI_I2S_FLAG){}
for SPI_I2S_FLAG_RXNE: Receive buffer not empty flag.
2017-10-04 10:45 AM
Hello.
So. .. this is not an SPI initialization problem.
Did you change also the porting functions concern SPI1 inside user_diskio.c file.?
Rgrds
vf
2017-10-04 12:03 PM
>>i am using stm32f070 device
Ok, but what is the *fully* qualified part number? Does the SPI2 clock enable stick in the APB1 register?
2017-10-04 11:54 PM
Hi Clive,
Yes SPI2 Clock enable in ABP1 register.
2017-10-04 11:57 PM
Hi,
i am not going to use any function of fatfs. i just enable SPI2 and send 0xFF to spi and wait for the response.
as you can see i am using only this function listed below.
uint8_t spi_rw8(uint8_t data){
while (SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_TXE) == RESET);SPI_SendData8(SPI2, data);while(SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_RXNE) == RESET); return SPI_ReceiveData8(SPI2);}2017-10-05 1:37 AM
Hello again.
As i understood code stops at the second while function (wait for RXNE).
It is not normal. Errata sheet not mention something similar.
If is possible, post CR1, CR2 and SR registers, when while loop stucks.
2017-10-05 7:56 AM
Hi,
register value is
CR1 = 0x0344
CR2 = 0x1700
SR = 0x0002
2017-10-05 12:03 PM
Hello again.
The values are normal. No interrupts enabled, no error flags, no DMA...
May be a faulty part .
If you have another board , check this issue to it.
At least, write some ''clean'' code that will includes only clocks and SPI2 initialization and spi_rw8(..) function called from main function. .
Post this code , post also the exact part type, so to have an answer from someone able to run the code to the same device.
Regards
vf