2008-04-14 12:57 AM
SPI1 Analog Devices AD7980 ADC problems
2011-05-17 03:29 AM
Hi,
Trying to talk to an Analog Devices AD7980 ADC using SPI1. Everything looks ok on the logic analyzer, but I'm not receiving any data on the MISO line. Does anybody have experience with these devices? I'm at my wits end. I use the library functions to set the SPI1 port up as a 16-bit master and handle the SS pin in hardware. Will post code if someone can help. Thanks2011-05-17 03:29 AM
2011-05-17 03:29 AM
Thanks Ivan,
Have you worked with this device before? It is indeed a strange interface, and there are various configurations possible. I also find the documentation a bit skimpy, unfortunately I'm taking this project over from someone else and I have to get the current hardware working. Any pointers/sample code/ docs would be greatly appreciated. Regards, André2011-05-17 03:30 AM