cancel
Showing results for 
Search instead for 
Did you mean: 

faster speed than 115200 with virtual com port or any other way?

hg-chen
Associate II
Posted on April 15, 2008 at 09:57

faster speed than 115200 with virtual com port or any other way?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
hg-chen
Associate II
Posted on May 17, 2011 at 12:30

Is there any way to reach speed more than baud rate 115200 with virtual com port?

or any other USB communication method between STM32 and PC can speed up and ready to use for people who do not know USB at all?

lanchon
Associate III
Posted on May 17, 2011 at 12:30

you could experiment with

http://www.st.com/mcu/forums-cat-6663-23.html

and test the speed.

16-32micros
Associate III
Posted on May 17, 2011 at 12:30

Go to function :UART0_Config in ''Hw.config.c'' and then comment the first condition as I have done here and Now it is working with higher baudrates that are enabled in your PC.

/*******************************************************************************

* Function Name : UART0_Config.

* Description : Configure the UART 0 according to the linecoding structure.

* Input : None.

* Return : Configuration status

TRUE : configuration done with success

FALSE : configuration aborted.

*******************************************************************************/

bool USART_Config(void)

{

/* set the bit rate*/

/*if ((linecoding.bitrate > 115200) || (linecoding.bitrate < 1200) )

{

USART_Config_Default();

return (FALSE);

}*/////////////////////////: Modified by STOne-32.

/* set the Stop bit*/

switch (linecoding.format)

{

case 0:

USART_InitStructure.USART_StopBits = USART_StopBits_1;

break;

case 1:

USART_InitStructure.USART_StopBits = USART_StopBits_1_5;

break;

case 2:

USART_InitStructure.USART_StopBits = USART_StopBits_2;

break;

default :

{

USART_Config_Default();

return (FALSE);

}

}

/* set the parity bit*/

switch (linecoding.paritytype)

{

case 0:

USART_InitStructure.USART_Parity = USART_Parity_No;

break;

case 1:

USART_InitStructure.USART_Parity = USART_Parity_Even;

break;

case 2:

USART_InitStructure.USART_Parity = USART_Parity_Odd;

break;

default :

{

USART_Config_Default();

return (FALSE);

}

}

/*set the data type : only 8bits and 9bits is supported */

switch (linecoding.datatype)

{

case 0x07:

USART_InitStructure.USART_WordLength = USART_WordLength_8b;

break;

case 0x08:

USART_InitStructure.USART_WordLength = USART_WordLength_9b;

break;

default :

{

USART_Config_Default();

return (FALSE);

}

}

USART_InitStructure.USART_BaudRate = linecoding.bitrate;

USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

USART_Init(USART1, &USART_InitStructure);

USART_Cmd(USART1, ENABLE);

return (TRUE);

}