2013-04-16 03:35 PM
I'm working with two STM32L151 communicating them via SPI port A-Master and B-Slave. I can only receive data correctly in B-Slave if I switch off transmission but I want full duplex in master and in slave. I can't either make the examples work properly. Has anybody had the same problem ?? I have attach the source code if someone wants to test it.
#forum-says-no #stm32l151-spi-slave2013-04-22 01:32 PM
I would like to know if someone has had the same problem?. Any idea why is not working properly ?
2013-04-22 07:20 PM
I have attach the source code if someone wants to test it.
Unfortunately your project is incomplete, using hardware and interfacing which isn't described. This would tend to limit the audience you're likely to attract, and the pool is already pretty shallow.