2015-09-21 7:52 AM
Hello,
I use a stm32f103, I want to use the SPI peripheral in slave mode.The SPI Master is configured with a clock at 1Mhz.I must to configure the STM32 SPI peripheral with a clock at 1Mhz, but its not possible with these prescalers availables, I can have 1.5Mhz or 0.75MKhz.Which clock I must choose ? the upper or the lower ?Thanks :) #spi-slave-mode #spi-stm32f1032015-09-21 8:28 AM
Pretty sure the slave shouldn't care, it's using the master's clock to shift the data, and the peripheral is clocking at the APB rate internally.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.