SPI reception, data shifted by one bit
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2012-06-08 8:42 AM
Hi,
I am having some difficulty receiving SPI data correctly and I am hoping someone could help.
I currently have two STM32L-Discovery boards connected via SPI with one acting as master and one as slave. My SPI transmissions from the master appear fine and I am able to see data being collected in the SPI receive buffer on the slave.
The problem I have is that there appears to be a shift in the received data, e.g:
If I Send:
'00110011'
I receive:
'01100110'
Similarly, if I send:
'01000110'
I receive:
'10001100'
I am pretty sure this is a clock polarity issue but having tried various different combinations of CPOL/CPHA on both the slave and master side, I am still unable to read back exactly what I have sent. Does anyone have any suggestions as to why this may be occurring? Is there anything aside from the CPOL/CPHA setup that I may be missing?
So that I do not add a whole pile of code, I have only added the SPI setups for master and slave. If any other info is required, I will gladly add to this.
-----
MASTER device
/**********************************************/
/* Configure SPI2 as transmitter */
/**********************************************/
SPI_I2S_DeInit(SPI2);
SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
SPI_InitStructure.SPI_Mode = SPI_Mode_Master;
SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;
SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low;
SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge;
SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;
SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2;
SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_LSB;
SPI_InitStructure.SPI_CRCPolynomial = 7;
SPI_Init(SPI2, &SPI_InitStructure);
SPI_I2S_ITConfig(SPI2, SPI_I2S_IT_TXE, ENABLE);
SPI_SSOutputCmd(SPI2, ENABLE);
SPI_Cmd(SPI2, ENABLE);
/*******************************************/
SLAVE device
/**********************************************/
/* Configure SPI2 as receiver */
/**********************************************/
SPI_I2S_DeInit(SPI2);
SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
SPI_InitStructure.SPI_Mode = SPI_Mode_Slave;
SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;
SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low;
SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge;
SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;
SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2;
SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_LSB;
SPI_InitStructure.SPI_CRCPolynomial = 7;
SPI_I2S_ITConfig(SPI2, SPI_I2S_IT_RXNE, ENABLE);
SPI_Cmd(SPI2, ENABLE);
/*******************************************/
---
Any suggestions/input would be greatly appreciated