cancel
Showing results for 
Search instead for 
Did you mean: 

SPI MISO and MOSI possible to communicate with Slave-SPI-IO (one Pin combined) on STM32F042K6T6 ?

NMich.1
Associate

My Slave got an update and has now a combined Pin for SPI-communication.

Before the Update, the Slave had MISO and MOSI Pins.

After Update, the Slave has one I/O-Pin for SPI-communication.

Is it somehow possible with the STM32F042K6T6 to communicate with its remaining two Pins MOSI and MISO?

So can i just connect both of them physically to the Slave-I/O ?

Is there an alternative possibility to communicate with the slave?

EDIT: alternative possibility means not I2C.. only SPI works for me.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0