2009-07-27 7:42 PM
spi master mode
2011-05-17 4:18 AM
Hi,
I´m using an stm32f103ret6, and i´m trying to read a temperature(ad7814) sensor by spi, but i already lose some days to put this work but spi doesn't cooperating, i'm already use a scopmeter and the sclk isn't generating by the stm. Can any one help me? this is my code and I do not know what could be wrong, i'm using stm32 in master mode and i just want to read from the sensor! /* SPI2 configuration ------------------------------------------------------*/ SPI_InitTypeDef SPI_InitStructure; /* Enable SPI2 */ SPI_Cmd(SPI2, ENABLE); //SPI_I2S_DeInit(SPI2); SPI_InitStructure.SPI_Direction =SPI_Direction_1Line_Rx; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_16b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_High; SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Hard; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_32; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_Init(SPI2, &SPI_InitStructure); while(1) { GPIO_WriteBit(GPIOB, GPIO_Pin_12, Bit_SET); delay( 1000000 ); GPIO_WriteBit(GPIOB, GPIO_Pin_12 ,Bit_RESET); while(SPI_I2S_GetFlagStatus(SPI2,SPI_I2S_FLAG_RXNE) != SET); ReceivedData = SPI_I2S_ReceiveData(SPI2); GPIO_WriteBit(GPIOB, GPIO_Pin_12, Bit_SET); //SPI_I2S_ClearFlag(SPI2, SPI_FLAG_CRCERR); temp_brut = ReceivedData; printf(''\r\n temp %d '',ReceivedData ); } //************ Configure SPI2 pins: SCK and MISO******************/ GPIOB_InitStructure.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_14 ; GPIOB_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIOB_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOB, &GPIOB_InitStructure); //************ Configure SPI2 pins: ~CS ******************/ GPIOB_InitStructure.GPIO_Pin = GPIO_Pin_12 ; GPIOB_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIOB_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(GPIOB, &GPIOB_InitStructure); best regards icosta2011-05-17 4:18 AM
Hello,
I think you have to enable the SPI1 clock like >RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI1, ENABLE); without that it should not run. You can look in the example SPI\Simplex_Interrupt\main.c in UM0427. And you also take a look at the NVIC configuration, for enable the IRQ Channel for the SPI interrupt. Perhaps this can help you. Patrick2011-05-17 4:18 AM
Sorry,
I mean the SPI2 clock of course for your case. Patrick2011-05-17 4:18 AM
You have to send something on the SPI in order to receive anything.
2011-05-17 4:18 AM
hi,
I don't post that part of code, but in the attach I have my main.c, and i enable the SPI2 clock like: /* Enable USART4 & SPI2 clocks */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART4 | RCC_APB1Periph_SPI2, ENABLE); Ivo Costa2011-05-17 4:18 AM
hi,
But i read my sensor data sheet and it isn't necessary send anything to work, i already use this sensor in fpga and the only thing that i did was enable de cs line and do the sclk, and the sensor send values, in the stm its necessary send messages even if it is not necessary for the sensor?because i analyze the sclk line and don't have anything! best regards ivo costa2011-05-17 4:18 AM
Lots ( most ) of the hardware SPI interfaces in uP's do not generate a clock if you don't send anything( write to the data register ). You could then of course send zero's .....
2011-05-17 4:18 AM
Quote:
Lots ( most ) of the hardware SPI interfaces in uP's do not generate a clock if you don't send anything
Agreed.Quote:
You could then of course send zero's ...
Or ones - depending on whether you expect the ''idle'' state of your MOSI line to be high or low... [ This message was edited by: st7 on 28-07-2009 08:14 ]