2025-02-05 03:25 AM
Hi everyone,
I'm working with the STM32L562 microcontroller and need to set up communication with the ADS8684 using SPI DMA. I am using SPI2, with the following pin configuration:
Could anyone guide me on how to implement SPI DMA to communicate with the ADS8684 efficiently? Any example code or advice would be greatly appreciated!
Thanks in advance!
2025-02-05 06:27 AM
Hello @NithinD and welcome to the community;
To start with SPI, I recommend you to look to some SPI_DMA examples may help you:
- SPI_FullDuplex_ComDMA_Master
I hope these resources help you.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.