cancel
Showing results for 
Search instead for 
Did you mean: 

Software packs for ARM V6.x (ArmClang) support

volker2
Associate II
Posted on March 29, 2018 at 07:58

Does anybody know, when software packs as example for Keil will be available that support the new ARM V6.x compiler/assembler?

For STM32F0x, STM32F1x and STM32F7x?

In the moment, the startup-files and parts of the c-code of the actual packs generate lots of errors while building a project.

Best regards

Volker

1 REPLY 1
volker2
Associate II
Posted on July 14, 2018 at 09:34

Although the actual packs include one file named cmsis_armcc_V6.h, they are not fully compatible to the ARM V6 toolchain. Neither the h. and c-Files nor the startup-Files from ST.

Also the CubeMX can`t generate Code for ARM V6.

Can anybody tell me when there will be a solution for this situation?

Best regards

Volker