2015-12-27 08:12 AM
Hi,
i am using nucleof103rb board, keil compiler. I have created 2 task in freeRTOS but only one task is getting executed.I tried but can't found the proper reason. --------------- Edited after posted ---------------------- I tried and i found it is problem with queueing. if i use queuesend and queuereceive then task get stuck at first task only. I have attached the updated code.#include ''stm32f1xx_hal.h''
#include ''cmsis_os.h''
UART_HandleTypeDef huart1;
xQueueHandle gbl_queue_handler=0;
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART1_UART_Init(void);
void StartDefaultTask(void const * argument);
void send_str1(void const * argument);
void send_str2(void const * argument);
void Sd_uart(void const * argument);
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_USART1_UART_Init();
HAL_UART_Transmit(&huart1,''Init'',4,1000);
gbl_queue_handler = xQueueCreate(6,sizeof(uint8_t));
xTaskCreate((TaskFunction_t)Sd_uart,''Suart'',256,NULL,1,NULL);
xTaskCreate((TaskFunction_t)send_str1,''string1'',256,NULL,1,NULL);
vTaskStartScheduler();
while (1)
{
}
}
/** System Clock Configuration
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = 16;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI_DIV2;
RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL16;
HAL_RCC_OscConfig(&RCC_OscInitStruct);
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2);
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}
/* USART1 init function */
void MX_USART1_UART_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
__GPIOA_CLK_ENABLE();
__USART1_CLK_ENABLE();
//tx
GPIO_InitStruct.Pin = GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
//rx
GPIO_InitStruct.Pin = GPIO_PIN_10;
GPIO_InitStruct.Mode = GPIO_MODE_AF_INPUT;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
huart1.Instance = USART1;
huart1.Init.BaudRate = 19200;
huart1.Init.WordLength = UART_WORDLENGTH_8B;
huart1.Init.StopBits = UART_STOPBITS_1;
huart1.Init.Parity = UART_PARITY_NONE;
huart1.Init.Mode = UART_MODE_TX_RX;
huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart1.Init.OverSampling = UART_OVERSAMPLING_16;
HAL_UART_Init(&huart1);
}
/** Configure pins as
* Analog
* Input
* Output
* EVENT_OUT
* EXTI
PA2 ------> USART2_TX
PA3 ------> USART2_RX
*/
void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
/* GPIO Ports Clock Enable */
__GPIOC_CLK_ENABLE();
__GPIOD_CLK_ENABLE();
__GPIOA_CLK_ENABLE();
__GPIOB_CLK_ENABLE();
/*Configure GPIO pin : PC13 */
GPIO_InitStruct.Pin = GPIO_PIN_13;
GPIO_InitStruct.Mode = GPIO_MODE_EVT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/*Configure GPIO pins : PA2 PA3 */
GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Speed = GPIO_SPEED_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*Configure GPIO pin : PA5 */
GPIO_InitStruct.Pin = GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Speed = GPIO_SPEED_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
}
void StartDefaultTask(void const * argument)
{
for(;;)
{
osDelay(1);
}
}
void send_str1(void const * argument)
{
uint8_t *dat=''Sagar'';
for(;;)
{
xQueueSend(gbl_queue_handler,dat,0);
GPIOA->ODR = 0x00000020;
taskYIELD();
}
}
void Sd_uart(void const * argument)
{
uint8_t *data;
xQueueReceive(gbl_queue_handler,data,100);
for(;;)
{
HAL_UART_Transmit(&huart1,''UART Task'',9,1000);
if(xQueueReceive(gbl_queue_handler,data,100))
{
HAL_UART_Transmit(&huart1,data,5,1000);
}
else
{
HAL_UART_Transmit(&huart1,''No Data'',7,1000);
}
taskYIELD();
}
}
#ifdef USE_FULL_ASSERT
void assert_failed(uint8_t* file, uint32_t line)
{
}
#endif
#nucleo
2015-12-27 11:53 AM
Not related, but toggling the GPIO might have more value
GPIOA->ODR ^= 0x00000020;