cancel
Showing results for 
Search instead for 
Did you mean: 

SImple question #ifndef __STM32F100_Dicovery_H

xtian
Associate II
Posted on January 18, 2013 at 02:11

what is this for

/**

  ******************************************************************************

  * @file    STM32vldiscovery.h

  * @author  MCD Application Team

  * @version V1.0.0

  * @date    09/13/2010

  * @brief   Header file for STM32vldiscovery.c module.

  ******************************************************************************

  * @copy

  *

  * THE PRESENT FIRMWARE WHICH IS FOR GUIDANCE ONLY AIMS AT PROVIDING CUSTOMERS

  * WITH CODING INFORMATION REGARDING THEIR PRODUCTS IN ORDER FOR THEM TO SAVE

  * TIME. AS A RESULT, STMICROELECTRONICS SHALL NOT BE HELD LIABLE FOR ANY

  * DIRECT, INDIRECT OR CONSEQUENTIAL DAMAGES WITH RESPECT TO ANY CLAIMS ARISING

  * FROM THE CONTENT OF SUCH FIRMWARE AND/OR THE USE MADE BY CUSTOMERS OF THE

  * CODING INFORMATION CONTAINED HEREIN IN CONNECTION WITH THEIR PRODUCTS.

  *

  * <h2><center>&copy; COPYRIGHT 2010 STMicroelectronics</center></h2>

  */

 

/* Define to prevent recursive inclusion -------------------------------------*/

 

&sharpifndef __STM32F100_Dicovery_H

 

&sharpdefine __STM32F100_Dicovery_H

//this one, is see this in every header... what is their function?

&sharpifdef __cplusplus

 extern ''C'' {

&sharpendif

/* Includes ------------------------------------------------------------------*/

&sharpinclude ''STM32f10x.h''

/** @addtogroup Utilities

  * @{

  */

 

/** @addtogroup STM32vldiscovery

#new-question-=-new-thread #include-guard #include-guard #include-guard #learning-c
This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
xtian
Associate II
Posted on January 18, 2013 at 16:41

thanks guys for your help.. additional question

/* GPIOA Periph clock enable */

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);

  /* Configure PA0 .. PA7 in output pushpull mode */

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

  GPIO_Init(GPIOA, &GPIO_InitStructure);

  /* Configure PA8 .. PA15 in input, pulled up mode */

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU;

  GPIO_Init(GPIOA, &GPIO_InitStructure);

  GPIOA->ODR = GPIOA->IDR >> 8; // Mirror high ordered inputs to low ordered outputs

could you explain to me the bold one especially ''8'' and IDR

Andrew Neil
Super User
Posted on January 18, 2013 at 16:58

You should start a new thread for a new question - otherwise the thread title becomes meaningless, and it all gets very confusing...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.