cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103ZF USB mass storage device problem

bikash
Associate II
Posted on January 18, 2013 at 17:35

Hello all,

         I am working on a project where I need to implement USB mass storage device.

 My SD card is communicating with controller on SPI2. As this microcontroller doesn't have the library for SPI so I used library code from STM32F103VBH6(eval board). But after integrating the code with my application I never get the device configured.I am new to USB don't know how to go with it.

My USB is running at 48MHz. and SPI at 400KHz.

D+ is permanently pulled high with 1.5k resistor.

Do I need to make any changes needs to be done in the code.

Please let me know where I am gone wrong.

Thanks in advance.

#stm32f103-usb-msd
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0