cancel
Showing results for 
Search instead for 
Did you mean: 

Short question regarding the contact drillings

timbo2023
Associate III

Good Morning Ladies and Gentlemen,

 

Could you communicate in a short way the size of the contact drill-holes (stm32f411 - CEU) ?

The diameter in AWG size would be enough.

We also are interested in further documentation-links regarding it.

 

In student words

"Have a nice day"

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

ST doesn't make that board, you'd need to ask the manufacturer.

 

But header pins plated through holes are typically around 1mm or 40mil, which is 18 AWG.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

9 REPLIES 9
waclawek.jan
Super User

What is "contact drills"?

Are you talking about some of the development boards, e.g. Nucleo?
JW

"drillings"

timbo2023
Associate III

"stm32f411ceu"

Hello @timbo2023 ,

Not sure I understood the question.

Could you please elaborate more or show image(s) or something similar to explain what you're talking about?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
timbo2023
Associate III

How many kind of holes to you see on a stm32f411ceu controller card?

Which diameter has this hole in "AWG-size"?

waclawek.jan
Super User
TDK
Super User

ST doesn't make that board, you'd need to ask the manufacturer.

 

But header pins plated through holes are typically around 1mm or 40mil, which is 18 AWG.

If you feel a post has answered your question, please click "Accept as Solution".
timbo2023
Associate III

ok