2026-04-03 12:20 AM
Dear al!
i need your help, i design PCB use STM32H755ZIT6, i set up mode PWR_SMPS_1V8_SUPLLY_LDO via STM32CubeMX 6.12.1. I expect core M7's clock is 400Mhz, M4's clock is 200Mhz. I measure voltage after L2 is 1.8V, at each Vcap pin is 1.0V, The MCU warmed up to about 35 degrees Celsius and chip didn't run. can you share me my mistake, this is the first time which i handle with SMPS block
2026-04-03 1:16 AM
Hi,
just...
- vbat not connected , connect to vdd.
- what is vddio ? should be 3v3 .
- whats on nrst ? should be 100nF to gnd.
+
What happens (if these voltages correct) on connecting in CubeProgrammer with st-link ?
show pic.
2026-04-03 1:22 AM
2026-04-03 2:06 AM
So connection to H755 cpu seems fine ? ...then cpu running.
Can you flash the cpu with success ?
So what means >chip didn't run< ? Your prog dont work ?
2026-04-03 3:45 AM
Could you please confirm:
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-04-03 6:27 PM