2016-08-02 03:06 PM
Hello
need to implement such a protocol i need to make solution without interrupts and with DMA the main idea is send bufer with timer like here but cant conigure timer may be exist better idea than using timer or may be somebody can help to configure timer thx2016-08-06 07:57 AM
Thx to all
__HAL_TIM_DISABLE(&htim8);
__HAL_TIM_DISABLE_DMA(&htim8, TIM_DMA_UPDATE);
HAL_DMA_Start_IT(htim8.hdma[TIM_DMA_ID_UPDATE], (uint32_t)&MASTER_BASE, (uint32_t)&GPIOA->BSRR, 74);
__HAL_TIM_ENABLE_DMA(&htim8, TIM_DMA_UPDATE);
__HAL_TIM_ENABLE(&htim8);