2016-04-13 03:37 AM
Hi,
I am using a STM32F429I discovery board. I have a running project in which I can generate code from STM32CubeMX. I would like to disable ''16-bit byte'', because I need the pin PE0 as a clock source for TIM4 (ETR2).The FMC controller for SDRAM2 is configured as follows:Clock and chip enable: SDCKE1+SDNEInternal bank numer: 4 banksAddress: 13 bitsData: 16 bits16-bit byte enableDoes anyone knows if this is possible?2016-04-14 05:22 AM
Hello,
Using CubeMX, it's possible to disable ''16-bit byte'' and enable the pin PE0 as a clock source for TIM4 (ETR2).I hope that answer your question, else you can provide more information about your issue.Regards-ForumSTM32-2016-04-14 06:07 AM
Its nicee
http://www.caraudiogiants.com/shop-by-category/speakers/soundstream-sst-20.html2016-04-14 06:23 AM
Hi jisa.sana,
The provided link is out of topic I think.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.