2016-09-04 01:02 AM
Hi,
I meet a problem with my project in which a STM32F373 MCU is used to collect singnal in single-ended mode.I short the pin with GND to test the board,the ADC values I get seems to fluctuate like saw-tooth.The graph above shows what I get with my board.The signal is moving averaged.But if I chang SDADC module into differential mode,the saw-tooth liked pattern disappears.The single passes through a RC network before it arrives at the SDADC pin.Has anyone encountered such a prolem?Thanks2016-09-06 06:00 PM