2017-11-25 4:06 AM
Hi.,
I am working on STM32F7 evolution board(Nucleo-F767ZI ) to interface external audio kit through SAI interface , I configured and got SAI drivers with STM cubeMX , The STM board is configured in Master mode with one block as transmitter and another as receiver(one block is working synchronously with another block ) and enabled the DMA to receive & transmit.
I can able to transmit data through SAI interface , but problem is with receiving . I am getting data for the first time through DMA , then onwards no data is receiving , same time I checked signals on board(FS,SCK & SD) all are coming but data is not receiving in to buffer. If I call SAI_DMAAbort() and then call receive function again data is receiving. What could be the problem. Should I need to abort DMA all the time or what.
SAI configurations:
hsai_BlockA1.Instance = SAI1_Block_A;
hsai_BlockA1.Init.AudioMode = SAI_MODEMASTER_TX; hsai_BlockA1.Init.Synchro = SAI_ASYNCHRONOUS; hsai_BlockA1.Init.OutputDrive = SAI_OUTPUTDRIVE_ENABLE; hsai_BlockA1.Init.NoDivider = SAI_MASTERDIVIDER_ENABLE; hsai_BlockA1.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_1QF; hsai_BlockA1.Init.AudioFrequency = SAI_AUDIO_FREQUENCY_48K; hsai_BlockA1.Init.SynchroExt = SAI_SYNCEXT_DISABLE; hsai_BlockA1.Init.MonoStereoMode = SAI_STEREOMODE; hsai_BlockA1.Init.CompandingMode = SAI_NOCOMPANDING; hsai_BlockA1.Init.TriState = SAI_OUTPUT_NOTRELEASED; if (HAL_SAI_InitProtocol(&hsai_BlockA1, SAI_I2S_STANDARD, SAI_PROTOCOL_DATASIZE_24BIT, 2) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }hsai_BlockB1.Instance = SAI1_Block_B;
hsai_BlockB1.Init.AudioMode = SAI_MODESLAVE_RX; hsai_BlockB1.Init.Synchro = SAI_SYNCHRONOUS; hsai_BlockB1.Init.OutputDrive = SAI_OUTPUTDRIVE_DISABLE; hsai_BlockB1.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_1QF; hsai_BlockB1.Init.SynchroExt = SAI_SYNCEXT_DISABLE; hsai_BlockB1.Init.MonoStereoMode = SAI_STEREOMODE; hsai_BlockB1.Init.CompandingMode = SAI_NOCOMPANDING; hsai_BlockB1.Init.TriState = SAI_OUTPUT_NOTRELEASED; if (HAL_SAI_InitProtocol(&hsai_BlockB1, SAI_I2S_STANDARD, SAI_PROTOCOL_DATASIZE_24BIT, 2) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }I have attached function calling detail documents for reference.
#nucleo-f767zi #stm32f72017-11-27 5:18 AM
Hi
karthikshivanna.94
,Have you try to start from SAI example under the STM32F7cube firmware package:
STM32Cube_FW_F7_V1.8.0\Projects\STM32756G_EVAL\Examples\SAI
-Nesrine-
2017-11-27 9:19 PM
Hai.,
I have taken same example project as reference , But I am getting lot of issues ,
>> I am not able continuously receive data through DMA(I need to call DMA abort every time before calling receive DMA function).
>> Also DMA receive call function effecting other global data buffers that I have defined.
I have attached part of initialization , Transmit & receive function calls in last thread , Can you please cross check and suggest if anything I am doing wrong.
Thank you.,
2017-12-06 6:24 PM
Did you set DMA up to circular buffer?
2017-12-06 9:24 PM
Hi Donald.,
No I haven't set DMA in circular mode , I chosen as normal mode.
2017-12-08 12:49 PM
If you want it to continuously transmit, you should use a circular buffer - otherwise you will have to tell the SAI every time you want to Rx data. You'll probably want to also use a 'ping-pong' or double-buffer scheme with your receiving location in memory by setting the half complete, and complete interrupts.
2017-12-08 9:51 PM
Hi Donald .,
Do you mean If I set in circular buffer no need to call receive function again and again . Once I call receive function then does it automatically all frames coming from SAI.
OK now I got some clarity to proceed further , If I suppose to set 8K bytes DMA receive mode , when half complete interrupt arrives then we can take first 4K buffer data and then so on.
Also I need some clarity what is maximum size I can set to DMA receive buffer. As per my above assumption will it support 8Kbytes size.
Thank you