cancel
Showing results for 
Search instead for 
Did you mean: 

RM0440, Rev 3, STM32G4 Reference Manual - Typos in HRTIM section 27.3.8

Singh.Harjit
Senior II

First sentence in the last paragraph says:

Up to 10 external event channels can be conditioned and are available simultaneously for

any of the 5 timers.

It should be 6 timers.

Actually, do a search for "5 timer" in Chapter 27 HRTIM and fix several locations that call out 5 timers instead of 6.

NOTE: use "5 timer" and not "5 timers" because there are places that are just timer.

Please also check the number of external event channels, etc. I didn't do that because I'm not very familiar with the implementation.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen GH
ST Employee

Hello,

Thank you, I will check

Best Regards

Imen GH
ST Employee

Hello,

Thank you for your contribution

I have raise your feedback internally for correction.

Regards