cancel
Showing results for 
Search instead for 
Did you mean: 

Ride7 Interrupts work in Flash but not RAM

smithdexter
Associate II
Posted on July 14, 2009 at 14:18

Ride7 Interrupts work in Flash but not RAM

2 REPLIES 2
smithdexter
Associate II
Posted on May 17, 2011 at 13:17

Hi,

I'm compiling a Timer interrupt example using Ride7 and downloading using RLink. When I select Flash I can happily get my timer interrupt and put a breakpoint on. However if I switch to RAM and change the settings on my STM3210E-EVAL board to SRAM - it compiles and downloads, but I don't get any interrupts. Any ideas what I'm doing wrong?

Dex

smithdexter
Associate II
Posted on May 17, 2011 at 13:17

Please any information will be helpful. I'm using the latest versions - downloaded 2 days ago. Does anyone know of problems with the default linker script? Is it because I'm using the standard version and need to upgrade to PRO?