Restart from SRAM after Bootloader with problems
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2012-06-30 12:40 AM
Posted on June 30, 2012 at 09:40
Hi guys,
i managed to flash my stm32f107vc via the internal bootloader, but i have problems to get the program running after it. When I reset the MCU the PC is somewhere at the beginning of SRAM i think (0x20000000). I found out, that if I set the PC to 0x8003000 manually, i can let the sw run and everything including interrupts works fine. Can someone help me how to manage to jump from 0x20000000 to 0x8003000 after reset? I am using a linkerfile as seen below:....
LR_IROM1 0x08003000 0x00080000-0x3000 { ER_IROM1 0x08003000 0x00080000-0x3000 { * (RESET, +First) .ANY (+RO) } IRAM 0x20000000 0xD800 ; 55296 Byte (10K also 10 Pages sind dahinter noch Platz) { *(STACK) .ANY2 (+RW +ZI) } .... before configuring the NVIC i call: NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x3000); thanks for your support guys! Toby
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2012-06-30 2:05 AM
Posted on June 30, 2012 at 11:05
Have you wired BOOT0 and BOOT1 correctly? They can be configured to boot from FLASH, embedded RAM or the ROM (''system memory'') boot loader. Please see AN2606, section 3.1.
TormodOptions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2012-06-30 2:02 PM
Posted on June 30, 2012 at 23:02
yes, sure. I have a jumper to select boot 0, boot 1.