cancel
Showing results for 
Search instead for 
Did you mean: 

Respiration Rate using stm32f429i discovery kit

lokesh
Associate II
Posted on February 11, 2015 at 11:27

I am just working on vital sign monitor project.

I have a stm32f429i discovery kit.

We are using capacitive sensor for respiratory signals, its very weak signals.

Sensor output will be fed to adc of microcontroller.

Which we need to pass thr' fft and band pass filter.

does anyone have idea of using fft and band pass filter together for medical application?

thanks in advance

#stm32f4 #discovery #vital-sign #respiratory
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
AvaTar
Lead
Posted on February 11, 2015 at 12:39

There is the DSP library for Cortex M, containing routines and example programs for FFT and filtering. There is at least one for the F40x, which is also be applicable to the F42x (never checked if there is one for the 42x, because I shun the ill-designed F429 discovery kit).

I am just working on vital sign monitor project.

 

I hope you have noticed the usual disclaimer at the last page of the MCU datasheet/reference manual:

ST PRODUCTS ARE NOT AUTHORIZED FOR USE IN WEAPONS. NOR ARE ST PRODUCTS DESIGNED OR AUTHORIZED FOR USE IN: (A) SAFETY CRITICAL APPLICATIONS SUCH AS LIFE SUPPORTING, ACTIVE IMPLANTED DEVICES OR SYSTEMS WITH PRODUCT FUNCTIONAL SAFETY REQUIREMENTS; (B) AERONAUTIC APPLICATIONS; (C) AUTOMOTIVE APPLICATIONS OR ENVIRONMENTS, AND/OR (D) AEROSPACE APPLICATIONS OR ENVIRONMENTS. ...