2011-07-24 03:52 AM
Hi,
My application would only run when I provide an external reset to my board (but when I use a JTAG debugger, it seems to work fine).
Is this a problem with the embedded power on reset? Do I need a delay at power-up?
2011-07-24 11:16 PM
Please check the h/w connections like VDD and GND tracks on the board.
2011-07-25 12:07 AM
Hi,
The problem was with the boot pins. There was a capacitor connected to one of the boot pins. This caused an incorrect value to be latched on the 4th rising edge of the system clock after reset.